Financial Releases
RFMD'S High-Performance CATV Amplifiers Receive "Product of the Year" Awards
Driven by explosive consumer demand for digital content, operators of multi-system networks are seeking more bandwidth, higher output, and lower distortion, while also requiring lower power consumption to reduce operating expenses. RFMD's award-winning CATV products leverage the Company's advanced compound semiconductor technologies, high-volume module assembly and industry-leading manufacturing scale to enable measurable improvements in efficiency, size, and performance.
"RFMD has proven its dedication to quality and excellence while addressing real needs in the marketplace. I am pleased to grant a 2011 Product of the Year Award for RFAM2790, RFCM2680, and RFPP2870," said
Cable Spotlight is a leading cable technology website. Their Third Annual Cable Spotlight Product of the Year Awards highlight innovative cable technology products brought to market in 2011.
Product Information:
-
RFAM2790. The RFAM2790 functions as an Edge QAM amplifier or a push-pull amplifier with +46dBmV output power. Its inner-stage attenuator provides 8-28dB gain range and it features power-down functionality for power save mode. The part meets DOCSIS 3.0 specifications with 7dB margin.
-
RFCM2680. The RFCM2680 is the world's first GaN-based surface mount power doubler. Capable of delivering +61dBmV output power, the RFCM2680 consumes 20% less current for the same linearity performance, compared to GaAs technology. The RFCM2680's surface mount package allows up to 50% savings in board area over industry-standard SOT115J packages.
- RFPP2870. The RFPP2870 is a GaN-based push-pull amplifier featuring high gain 28dB (minimum at 1003MHz) and excellent linearity at low distortion levels. It is available in an industry-standard SOT115J package.
About TMC
TMC, celebrating its 40th Anniversary in 2012, is a global, integrated media company that helps clients build communities in print, in person, and online. TMC publishes the Customer Interaction Solutions, INTERNET TELEPHONY, Next Gen Mobility and Cloud Computing (formerly InfoTECH Spotlight) magazines. TMCnet.com, which is read by 1.5 million unique visitors each month, is the leading source of news and articles for the communications and technology industries. TMC is the producer of ITEXPO, the world's leading B2B communications event. In addition, TMC runs multiple industry events: including Mobility Tech, M2M Evolution, Business Video, ChannelVision Expo, MSPWorld, Super WiFi, SUITS, LatinComm, HTML5 Summit Conferences and more. Visit TMC Events for a complete listing and further information. For more information about TMC, visit www.tmcnet.com.
About Cable Spotlight
Cable Spotlight is the leading Website dedicated to cable technologies. The site provides the latest news, reviews and resources. Tailored specifically for cable technology and communications, visitors will find the most daily content delivering relevant cable industry news, blogs, feature articles, white papers, videos and more. Cable Spotlight is owned and operated by TMC. Visit www.cable.tmcnet.com.
About RFMD
Headquartered in
The
This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws.
RF MICRO DEVICES®, RFMD® and PowerSmart® are trademarks of
CONTACT: At RFMD(R)Doug DeLieto VP, Investor Relations 336-678-7088
Source:
News Provided by Acquire Media