Financial Releases
RFMD(R) Teams With Silicon Labs to Deliver High-Performance Sub-GHz Solution for Smart Energy Applications
The RFMD® RF6569 smart energy front-end module (FEM) and Silicon Labs' EZRadioPRO® Si4464/63 transceivers have been combined to create the RF6569/Si4464/63 reference design. This high-performance Sub-GHz solution provides public utilities and consumers more control over how they monitor and save energy. The solution targets portable battery-powered equipment such as smart energy advanced metering infrastructure, security and home automation systems, industrial control systems, and sensor networks in the 902 to 928MHz and 868MHz ISM bands.
RFMD's highly integrated RF6569 module features a 915MHz/868MHz 30dBm power amplifier, a Tx harmonic output filter, a single-pole double—throw (SPDT) antenna switch, and an Rx through path. The RF6569 is housed in a 5.5 x 5.0 x 1mm package, reducing discrete component content while minimizing footprint and assembly costs. The transceiver interface is single-ended with separate Rx/Tx.
"The combination of RFMD's RF6569 module and Silicon Labs' Si446x EZRadioPRO provides an energy-efficient solution for long-range RF applications such as smart utility metering," said
For more information about the RF6569/Si4464/63 reference design (part number 4463-TCE30E915R-EK), visit http://www.rfmd.com/products/siliconlabs/rf6569-si4464.aspx.
About the EZRadioPRO Wireless IC Family
Silicon Labs' EZRadioPRO family of transmitters, receivers and transceivers extends all the benefits of the EZRadio® family, such as high integration, low cost, flexibility and easy design-in, into more sophisticated ISM band applications. EZRadioPRO devices offer an array of enhanced parameters and features including continuous frequency coverage from 119 to 1050 MHz and output power up to +20 dBm. They also include useful built-in features such as wake-up timer, low battery detector, transmit and receive data FIFOs, power-on reset circuit and general-purpose digital I/Os. For more information about Silicon Labs' EZRadioPRO family, visit www.silabs.com/EZRadioPRO.
Silicon Laboratories Inc.
Silicon Laboratories is an industry leader in the innovation of high-performance, analog-intensive, mixed-signal ICs. Developed by a world-class engineering team with unsurpassed expertise in mixed-signal design, Silicon Labs' diverse portfolio of patented semiconductor solutions offers customers significant advantages in performance, size and power consumption. For more information about Silicon Labs, please visit www.silabs.com.
About RFMD
Headquartered in
The
This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of
these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws.
RF MICRO DEVICES® and RFMD® are trademarks of
CONTACT: At RFMD(R)
Doug DeLieto
VP, Investor Relations
336-678-7088
At Silicon Laboratories (R)
Dale Weisman
Global PR Manager
512-532-5871
Source: News Provided by Acquire Media