Financial Releases
TriQuint Portfolio Supports Industry's Move To More Efficient Base Station Networks
TriQuint’s new base station modules offer designers four levels of RF integration to reduce board space, lower bill of materials, and improve efficiency. Level 1 TriQuint solutions include high gain products that can replace one or more discrete components with a single module. At the highest level of integration, TriQuint’s new Level 4 modules such as the TQM879006, replace multiple discrete products with one module that incorporates two amplifiers, a digital step attenuator and all input/output matching circuitry.
“Global mobile networks are transitioning to base stations that use remote radio head designs. TriQuint’s newest products simplify RF connectivity in these systems. TriQuint devices enable manufacturers to focus on competitive system performance instead of dedicating valuable resources toward RF component matching issues,” said Brian P. Balut, TriQuint Vice President.
Huawei Networks touts the benefits of remote radio head designs in both trial and operational systems. In work with international mobile operator Vodaphone, Huawei notes in an article entitled, “Network Deployment; it’s all in the mind,” that the cost savings from increased efficiency in the links between the base station and the rest of the network are very significant. Remote radio head innovations are central to moving all key radio components closer to the antenna while reducing the size of radio housings; these advances reduce power consumption directly and through lower overall thermal mitigation requirements.
TriQuint base station customers including Samsung Electronics have benefitted from the space-saving and cost reduction benefits of integrated components.
“We appreciate the quality of TriQuint’s AH212 and AH420. These devices have enabled us to develop high power amplifiers for new LTE base station systems. The support we receive from TriQuint has helped us satisfy customer demands,” said Samsung Electronics RF Core Lab Senior Engineer, Jong-Hyun Lee.
Leading base station repeater manufacturer SK-Telesys also recognizes the benefits of TriQuint components in their WCDMA and CDMA systems.
“Our experience with TriQuint’s products including the AH212, AH225 and the ML485 has been very good. These devices enabled us to develop new repeater systems. Engineering and product support from TriQuint have been important for us in meeting customer deadlines and requirements,” said SK-Telesys Access R&D Senior Engineer, Chul Lee.
TriQuint products are used by major OEM base station radio manufacturers across Europe, Asia and North America in WCDMA, CDMA, MC-GSM and LTE networks. TriQuint’s newest, fully-integrated base station module, the TQM879006, is being released in conjunction with the 40th Annual European Microwave Conference, in Paris, France (28-30 September 2010); visit TriQuint at Stand 60.
Technical Details
TriQuint offers integrated pre-driver and driver RFIC base station solutions designed to improve efficiency, reduce the PCB area dedicated to RF and reduce remote radio head bill of materials. TriQuint’s base station portfolio includes gain blocks, switches, mixers, low noise and driver amplifiers, converters, SAW filters and integrated modules.
TriQuint’s Pre-Driver and Driver Integrated Products
Level 1 |
Devices that offer higher gain than discrete components and integrated matching. This eliminates one or more components in base station amplifier line-ups for size and overall cost savings. Example: TQP3M9008, TQP3M9009 |
Level 2 |
Devices that integrate multiple functions in a package such as a multi-stage amplifier or mixer and an LO buffer amplifier for reduced system size. Example: TQP8M9013, ML483, ML485 |
Level 3 |
Devices that combine two complete amplifier stages and interstage matching. These products eliminate the need for matching circuits between amplifiers while reducing costs and circuit size. Example: AH212, AH323 |
Level 4 |
Full integration at 50 Ohm input/output impedance. Multiple functions incorporated into a package such as two amplifiers, a digital step attenuator, all bias chokes as well as bypass and blocking capacitors that yields a simpler, more compact solution for lower overall costs. Example: TQM879006 |
For more information about TriQuint’s new base station products, point-to-point microwave, optical networks, defense/aerospace, foundry and mobile device solutions, contact TriQuint Product Marketing or visit us on the web at: www.triquint.com. For information about future product releases and to subscribe to our newsletter, visit www.triquint.com/rf.
FORWARD LOOKING STATEMENTS
This TriQuint Semiconductor, Inc. (NASDAQ: TQNT) press release contains forward-looking statements made pursuant to the Safe Harbor provisions of the Private Securities Litigation Reform Act of 1995. Readers are cautioned that forward-looking statements involve risks and uncertainties. The cautionary statements made in this press release should be read as being applicable to all related statements wherever they appear. Statements containing such words as ‘leading’, ‘exceptional’, ‘high efficiency’, ‘key role’, ‘leading supplier’, or similar terms are considered to contain uncertainty and are forward-looking statements. A number of factors affect TriQuint’s operating results and could cause its actual future results to differ materially from any results indicated in this press release or in any other forward-looking statements made by, or on behalf of, TriQuint including, but not limited to: those associated with the unpredictability and volatility of customer acceptance of and demand for our products and technologies, the ability of our production facilities and those of our vendors to meet demand, the ability of our production facilities and those of our vendors to produce products with yields sufficient to maintain profitability, as well as the other “Risk Factors” set forth in TriQuint’s most recent 10-Q report filed with the Securities and Exchange Commission. This and other reports can be found on the SEC web site, www.sec.gov. A reader of this release should understand that these and other risks could cause actual results to differ materially from expectations expressed / implied in forward-looking statements.
FACTS ABOUT TRIQUINT
TriQuint Semiconductor (NASDAQ: TQNT) celebrates its 25th anniversary in 2010 as a leading global provider of innovative RF solutions and foundry services for the world’s leading communications, defense and aerospace companies. People and organizations around the world need real-time, all-the-time connections; TriQuint products help reduce the cost and increase the performance of connected mobile devices and the networks that deliver critical voice, data and video communications. With the industry’s broadest technology portfolio, recognized R&D leadership, and expertise in high-volume manufacturing, TriQuint creates standard and custom products using gallium arsenide (GaAs), gallium nitride (GaN), surface acoustic wave (SAW) and bulk acoustic wave (BAW) technologies. The company has ISO9001-certified manufacturing facilities in the U.S., production in Costa Rica, and design centers in North America and Germany. For more information, visit www.triquint.com.
TriQuint: Connecting the Digital World to the Global Network®
TriQuint Product Marketing: |
TriQuint Media Contact: |