Financial Releases

RFMD(R) Adds WLAN Front-End Module for Handsets to Industry-Leading Portfolio of Power Amplifiers; RF5924 Optimizes Size, Power Output, And Linearity For Embedded WLAN Applications In Handsets

RFMD(R) Adds WLAN Front-End Module for Handsets to Industry-Leading Portfolio of Power Amplifiers; RF5924 Optimizes Size, Power Output, And Linearity For Embedded WLAN Applications In HandsetsLAS VEGAS--(BUSINESS WIRE)--April 5, 2006--RFMD® (NASDAQ: RFMD), a leading provider of proprietary radio frequency integrated circuits (RFICs) for wireless communications applications, today announced volume shipments of the RF5924, the industry's first front-end module (FEM) designed specifically for embedded wireless LAN (WLAN) applications in cellular handsets.

RFMD's RF5924 is a complete front-end module that requires no external components, enabling the smallest footprint area of any 802.11g front-end module on the market today. Featuring a WLAN power amplifier (PA), switch and receive balun, the RF5924 provides all the required functions between the RF transceiver and the system BPF/antenna. With all RF ports 50-ohm matched, the RF5924 is designed to ease system implementation and reduce product development time.

"RFMD is leveraging its leadership in cellular power amplifiers and extending it into the WLAN power amplifier market," said Rohan Houlden, Director of RFMD's Network Components Product Line. "The RF5924 is the first offering in a dedicated line of mobile WLAN components that address all bands and standards and continue RFMD's heritage of delivering industry-leading technology to emerging, high-growth markets."

Designed for easy integration into mobile phones, personal digital assistants (PDAs), and other portable battery powered devices, the RF5924 provides higher data throughput and greater WLAN coverage. The performance characteristics of the RF5924 specifically address the requirements of advanced wireless applications, such as Voice over Internet Protocol (VoIP), which are driving the adoption of WLAN in handsets and the creation of new WLAN standards.

    Key features of the RF5924 include:

    --  Package: 3.5x3.5x1.4mm module

    --  Pout=16dBm, 11g, OFDM<3.3% EVM

    --  Direct battery connection

    --  Single 3.1V to 4.5V supply voltage

    --  Integrated 2.5GHz b/g amplifier, RX balun and switch

    --  Bluetooth(R) port - shared antenna between WLAN and Bluetooth
        systems

The RF5924 is priced at $1.74 in quantities of 10,000 units. For additional information, contact RFMD by phone (336) 678-5570 or FAX (336) 664-0292 or visit the Company's Web site at www.rfmd.com.

RFMD will be showcasing its WLAN FEM products and other wireless solutions at CTIA Wireless 2006 in Las Vegas, Nevada, April 5-7, 2006, in Booth 1036.

About RFMD

RFMD, an ISO 9001- and ISO 14001-certified manufacturer, designs, develops, manufactures and markets proprietary radio frequency integrated circuits (RFICs) for wireless communications products and applications. The Company is a leading supplier of power amplifiers, one of the most critical radio frequency (RF) components in cellular phones. The Company is also the leading manufacturer of GaAs HBT, which offers distinct advantages over other technologies for the manufacture of current- and next-generation power amplifiers. The Company's products are included primarily in cellular phones, base stations, wireless local area networks (WLANs), cable television modems and global positioning systems (GPS). The Company derives revenue from the sale of standard and custom-designed products. The Company offers a broad array of products including amplifiers, mixers, modulators/demodulators and single-chip transmitters, Bluetooth® products and receivers and transceivers that represent a substantial majority of the RFICs required in wireless subscriber equipment. The Company's goal is to be the premier supplier of low-cost, high-performance integrated circuits and solutions for applications that enable wireless connectivity. RFMD is traded on the Nasdaq National Market under the symbol RFMD. For more information about RFMD, please visit www.rfmd.com.

This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. RF Micro Devices' business is subject to numerous risks and uncertainties, including variability in quarterly operating results, the rate of growth and development of wireless markets, risks associated with the operation of our wafer fabrication facilities, molecular beam epitaxy facility, our assembly facility and our test, tape and reel facilities, our ability to attract and retain skilled personnel and develop leaders, variability in production yields, our ability to reduce costs and improve gross margins by implementing innovative technologies, our ability to bring new products to market, dependence on consignment sales through customer inventory hubs, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, dependence on a limited number of customers, dependence on third parties and the variability of future stock-based compensation charges or credits during the remainder of fiscal 2006 as a result of our stock option exchange program as well as the adoption of SFAS 123® in fiscal 2007. These and other risks and uncertainties, which are described in more detail in RF Micro Devices' most recent Annual Report on Form 10-K filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

RF MICRO DEVICES® and RFMD® are trademarks of RFMD, LLC. BLUETOOTH is a trademark owned by Bluetooth SIG, Inc., U.S.A. and licensed for use by RF Micro Devices, Inc. All other trade names, trademarks and registered trademarks are the property of their respective owners.

CONTACT: RFMD
Jerry Neal or Doug DeLieto, 336-664-1233

SOURCE: RFMD®