Financial Releases

RFMD(R) Introduces Transmit System for 3G Handsets

RFMD(R) Introduces Transmit System for 3G Handsets Flexible UMTS Solution Simplifies Implementation of Multi-Region Multimode 3G Handset Platforms

BARCELONA, Spain--(BUSINESS WIRE)--Feb. 12, 2007--RF Micro Devices, Inc. (NASDAQ: RFMD), a global leader in the design and manufacture of high-performance radio systems and solutions for applications that drive mobile communications, today announced the RF628x family of products, which combine to provide a UMTS transmit system for the implementation of multi-region multimode 3G handset platforms.

RFMD's UMTS transmit system supports all major UMTS frequency bands and is comprised of the RF6280 (announced separately today), RF6281 and RF6285. The transmit system features a dedicated single-band power amplifier module (supporting Band I), a flexible dual-band power amplifier module (capable of supporting Bands I, II, III, IV, V, VI, VIII, IX) and a low-noise, high efficiency DC to DC converter/controller. The compact design of the RF628x transmit system enables a greater than 30% reduction in the implementation of tri-band UMTS solutions, including filtering, as compared to competitive solutions.

By leveraging the broadband characteristics of the dual-band RF6285, the transmit system greatly simplifies the implementation of multimode, multi-region 3G handset platforms. In addition, by leveraging a balanced PA architecture, the transmit system provides improved total radiated power (TRP) and specific absorption rate (SAR) performance, which eliminates the need for costly RF isolators and also greatly simplifies platform implementation.

RFMD's transmit system offers best-in-class efficiency through the use of analog bias control and the RF6280 DC to DC converter/controller, which maximize efficiency across all power levels and data rates (voice-only to HSPA). This helps to extend talk time and reduces thermal dissipation, both of which are critical customer metrics.

Konrad Alvarino, general manager of RFMD's components business unit, said, "The RF6280, RF6281 and RF6285 UMTS transmit system strengthens RFMD's position as the number one supplier of UMTS power amplifiers. Importantly, RFMD's UMTS transmit system provides our customers the flexibility to design a single platform that supports multiple UMTS regions by simply changing filter components. No change to the phone board's RF layout is necessary. When combined with the benefits of improved TRP and SAR and best-in-class efficiency, the transmit system delivers a compelling solution to customers seeking a cost-effective and highly efficient flexible UMTS platform."

Total radiated power (TRP) is the measure of a mobile device's radiated output power. TRP is a function of the output power of the power amplifier, the antenna's radiation efficiency and the power amplifier's sensitivity to antenna mismatch. Antenna mismatch occurs in all handsets and is more predominant in multi-band "worldphones" because of the increase in the number of bands supported by the antenna. As a result of antenna mismatch, handsets can operate below planned output power, resulting in dropped calls, or above planned output power, resulting in reduced talk time and poor call quality. Improvements in TRP increase network efficiency, network coverage and data throughput rates while also reducing the frequency of dropped calls. RFMD has shipped approximately 20 million power amplifiers to date that reduce variation in output power into mismatched antennas and deliver industry-leading TRP performance.

RFMD forecasts the 3G multimode market will exceed 500 million handsets by 2010, reflecting a compound annual growth rate approaching 40%. Additionally, RFMD estimates that the number of UMTS frequency bands supported by the average 3G multimode device will approximately double by 2010. RFMD is the global leader in UMTS power amplifiers.

The RF6280, RF6281 and RF6285 all comply with the Restriction of Hazardous Substances Directive (RoHS) and will be available for sampling in the third quarter of 2007.

About RFMD: RF Micro Devices, Inc. (NASDAQ: RFMD) is a global leader in the design and manufacture of high-performance radio systems and solutions for applications that drive mobile communications. RFMD's power amplifiers, transmit modules, cellular transceivers and system-on-chip (SoC) solutions enable worldwide mobility, provide enhanced connectivity and support advanced functionality in current- and next-generation mobile handsets, cellular base stations, wireless local area networks (WLANs) and global positioning systems (GPS). Recognized for its diverse portfolio of state-of-the-art semiconductor technologies and vast RF systems expertise, RFMD is a preferred supplier enabling the world's leading mobile device manufacturers to deliver advanced wireless capabilities that satisfy current and future market demands.

Headquartered in Greensboro, N.C., RFMD is an ISO 9001- and ISO 14001-certified manufacturer with worldwide engineering, design, sales and service facilities. RFMD is traded on the NASDAQ Global Select Market under the symbol RFMD. For more information, please visit RFMD's web site at www.rfmd.com.

This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. RF Micro Devices' business is subject to numerous risks and uncertainties, including variability in quarterly operating results, the rate of growth and development of wireless markets, risks associated with the operation of our wafer fabrication facilities, molecular beam epitaxy facility, assembly facility and test and tape and reel facilities, our ability to attract and retain skilled personnel and develop leaders, variability in production yields, our ability to reduce costs and improve gross margins by implementing innovative technologies, our ability to bring new products to market, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, dependence on a limited number of customers, and dependence on third parties. These and other risks and uncertainties, which are described in more detail in RF Micro Devices' most recent Annual Report on Form 10-K filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

RF MICRO DEVICES® and RFMD® are trademarks of RFMD, LLC. All other trade names, trademarks and registered trademarks are the property of their respective owners.

CONTACT: RF Micro Devices, Inc.
Kevin Walsh, 978-670-2212
Director of Business Development
or
Doug DeLieto, 336-678-5091
Vice President, Investor Relations

SOURCE: RF Micro Devices, Inc.