Financial Releases
RFMD(R) Expands High-Performance RF Switch Portfolio
The RF1126 is a low-power, single-pole double-throw (SPDT) symmetric switch that offers industry-leading insertion loss and linearity performance suitable for signal routing and antenna switching applications. The RF1131 and RF1132 are single-pole three-throw (SP3T) symmetric switches designed for applications requiring high linearity performance, such as CDMA handsets and 3G multimode devices. The RF1131 and RF1132 are pin-for-pin compatible and offer performance trade-offs between linearity and insertion loss, enabling designers to select a switch based upon a specific application's performance priorities, thereby increasing platform capabilities.
Each of the three RF switches utilize RFMD's industry-leading gallium arsenide (GaAs) pseudomorphic high electron mobility transistor (pHEMT) manufacturing capabilities and leverage proprietary switch technology developed for use in RFMD's high volume cellular transmit modules.
Technical features of the RF1126:
-- Very small footprint, 2.0 x 1.3 x 0.35 mm QFN package
-- Very low insertion loss
-- Ideal for use in multi-band CDMA Rx diversity applications
Technical features of the RF1131 and the RF1132:
-- Very small footprint: 2.0 x 2.0 x 0.55 mm QFN package
-- Low insertion loss: RF1131 - 0.32 to 0.49 dB, RF1132 - 0.47 to 0.69 dB
-- Excellent Linearity (IIP3): RF1131 - 59 dBm (Cell) / 62 dBm (PCS),
RF1132 - 65 dBm (Cell) / 63 dBm (PCS)
-- Ideal for use in multi-band CDMA single routing applications
Availability
Samples of the RF1126, RF1131 and RF1132 are available immediately. RFMD® anticipates revenue generated by its switch portfolio to grow throughout calendar year 2009.
RFMD will showcase its industry-leading portfolio of cellular front end
products at the 2009
RFMD's Cellular Front End Components Portfolio
RFMD offers a broad portfolio of high-performance front end components addressing the increasingly complex challenges of the cellular market. RFMD's front end components address all cellular frequency bands and air standards and include discrete switches, antenna switch modules, LNAs, front end power management and RF power management.
About RFMD
Headquartered in
This press release includes "forward-looking statements" within the
meaning of the safe harbor provisions of the Private Securities Litigation
Reform Act of 1995. These forward-looking statements include, but are not
limited to, statements about our plans, objectives, representations and
contentions and are not historical facts and typically are identified by use
of terms such as "may," "will," "should," "could," "expect," "plan,"
"anticipate," "believe," "estimate," "predict," "potential," "continue" and
similar words, although some forward-looking statements are expressed
differently. You should be aware that the forward-looking statements included
herein represent management's current judgment and expectations, but our
actual results, events and performance could differ materially from those
expressed or implied by forward-looking statements. We do not intend to update
any of these forward-looking statements or publicly announce the results of
any revisions to these forward-looking statements, other than as is required
under the federal securities laws.
RF MICRO DEVICES® and RFMD® and POLARIS® are trademarks of
SOURCE
CONTACT: Doug DeLieto VP, Investor Relations, 1-336-678-7968, or
Jerry
Neal
both of RFMD
Web Site: http://www.rfmd.com
(RFMD)