Financial Releases
RFMD(R) Expands Front End Module Portfolio for Mobile Wi-Fi Market
The RF5325, RF5345, and RF5725 FEMs each contain a 2.4 GHz power amplifier (PA) designed to optimize linearity while minimizing current consumption--a critical requirement in battery powered devices. Each FEM integrates an output power coupler, transmit (Tx) low pass filtering and a single-pole three-throw (SP3T) switch capable of switching between Wi-Fi receive (Rx), Wi-Fi Tx, and Bluetooth® Rx/Tx operations. The integrated coupler significantly lowers bill-of-material (BOM) costs and reduces the board area necessary for front end implementation in chipsets utilizing closed loop power control to adjust output power. The RF5345 and RF5725 also integrate a low noise amplifier (LNA) for RF architectures requiring additional Rx gain.
"We are very pleased to expand our portfolio of Wi-Fi front ends to
address the growing opportunities in Wi-Fi-enabled mobile devices," said
Technical features of the RF5325, RF5345, and RF5725 include:
-- Compact, low profile packages: 3.0 x 3.0 x 0.5 mm
-- Low external component count
-- Designed for operation in 802.11 b/g/n systems
-- Excellent linearity, 3.3% error vector magnitude (EVM)
-- Integrated output power coupler
RFMD's Wi-Fi and WiMAX Front End Portfolio
RFMD delivers a broad product portfolio enabling Wi-Fi and WiMAX connectivity across multiple applications, including handsets, consumer electronics, desktop and laptop computers, client access cards, wireless access points, routers, consumer premises equipment (CPE) and base transceiver stations (BTS). RFMD's high performance Wi-Fi and WiMAX products encompass all 802.11a/b/g/n and 802.16 applications and include amplifiers, power amplifiers, low noise amplifiers, switches and highly integrated front end modules.
Availability and Pricing
Samples of the RF5325, RF5345, and RF5725 are available immediately, and RFMD anticipates revenue generated by its Wi-Fi front end portfolio to grow throughout calendar year 2009. Pricing is available upon request by contacting an RFMD sales representative or by visiting www.rfmd.com/purchase.
RFMD's product portfolio will be on display at the 2009 GSMA Mobile World
Congress
About RFMD
Headquartered in
This press release includes "forward-looking statements" within the
meaning of the safe harbor provisions of the Private Securities Litigation
Reform Act of 1995. These forward-looking statements include, but are not
limited to, statements about our plans, objectives, representations and
contentions and are not historical facts and typically are identified by use
of terms such as "may," "will," "should," "could," "expect," "plan,"
"anticipate," "believe," "estimate," "predict," "potential," "continue" and
similar words, although some forward-looking statements are expressed
differently. You should be aware that the forward-looking statements included
herein represent management's current judgment and expectations, but our
actual results, events and performance could differ materially from those
expressed or implied by forward-looking statements. We do not intend to update
any of these forward-looking statements or publicly announce the results of
any revisions to these forward-looking statements, other than as is required
under the federal securities laws.
RF MICRO DEVICES® and RFMD® and POLARIS® are trademarks of
SOURCERF Micro Devices, Inc. -0-02/16/2009 /CONTACT: Doug DeLieto, VP, Investor Relations, +1-336-678-7968, orJerry Neal , Executive Vice President, +1-336-678-7001, both of RFMD/ /Web Site: http://www.rfmd.com / (RFMD) CO:RF Micro Devices, Inc. ;GSMA Mobile World Congress ST:North Carolina ,Spain IN: CPR HRD NET ITE SU: PDT TDS PR -- NY71129 -- 112902/16/2009 01:35 EST http://www.prnewswire.com