Financial Releases

TriQuint Semiconductor's Filter For High Performance Cable Modems Doubles Available Bandwidth

SHENZHEN, CHINA & HILLSBORO, OR (USA) – March 3rd, 2008 – TriQuint Semiconductor (Nasdaq: TQNT), a leading RF semiconductor manufacturer and foundry services provider, today announced the release of its newest filter for high-speed wideband cable television digital tuner applications. The filter, built using a newly developed proprietary technique, has enabled CATV tuner, baseband and set-top box (STB) manufacturers to build smaller, high performance DOCSIS® 3.0-based high-speed cable modems. These modems are optimized for faster data transfer including advanced services such as video on demand (VOD).

TriQuint believes this filter is a first-of-its-kind development in the digital tuner/cable market since previous application-specific filters at the same center frequency offered half the fractional bandwidth of TriQuint’s new device. This breakthrough technology is a result of close cooperation between TriQuint’s research, product development and manufacturing teams as well as other industry leaders.

“Using a SAW filter for the 1st IF stage in our tuner design was a critical step to achieving a design that can ramp quickly to high volumes,” said Carey Ritchey, Director of Broadband Systems, Microtune®, Inc. “Our positive working relationship has produced key DOCSIS 3.0 technology that, when integrated into cable modems, permits service providers to offer bandwidth-hungry consumers ultra-fast cable telecommunications services.”

TriQuint’s new surface acoustic wave (SAW) intermediate frequency (IF) filter was introduced in Shenzhen, China today during the 13th Annual International IC-China Conference and Exhibition. Each year this event introduces the latest advancements in electronics engineering to manufacturers and suppliers in major cities across China. The 2008 event is being held February 28 to March 11 in Chengdu, Shenzhen, Beijing and Shanghai.

The DOCSIS 3.0 specification, the fourth generation of the cable industry’s data over cable service interface application specification, was created to enable faster two-way movement of large data files over conventional hybrid fiber coax (HFC) cable. The new specification was also designed to help cable service operators compete effectively with other broadband, high-speed systems such as DSL (digital subscriber line) access, IP over Satellite (IPoS) links or optical fiber-based systems. Delivering faster two-way access over the HFC cable required new generations of digital tuners that in turn required advanced filter technology. TriQuint believes that it is the first to satisfy this demand with an economical, SAW-based solution.

“TriQuint innovation is helping digital tuner designers realize the promise of DOCSIS 3.0 technology,” remarked TriQuint Asia Sales Director, Richard Lin. “TriQuint helped take the potential for faster transfer of larger data files and make it a reality. This new technology and work with our chipset partners demonstrates how dynamic an established technology like SAW can be and how a company can enable progress across an entire market segment.”

“TriQuint's new DOCSIS 3.0-based SAW filter gives us the necessary performance and cost metrics to develop a compelling solution for both our high-speed data chipset and our TeraPIX Video Processor" said BroadLogic Director of Product Marketing, Giri Venkant. "TriQuint worked very closely with us during the development program, even helping with on-board optimization in the early stages to help ensure its success."

According to market research group Strategy Analytics, the cable market is continuing to grow at a high rate, driven by governmental mandates for conversion to digital signals in China, the United States and elsewhere. China Digital TV, which has a 44% share of the Chinese market1, projects the digital access card market will grow in China from 8.7 million in 2006 to 45.9 million by 2010.

Manufacturers and cable service providers are already touting hardware and service enhancements designed to take advantage of DOCSIS 3.0 network capabilities. At CES—the 2008 Consumer Electronics Show in Las Vegas, USA, a consortium of equipment manufacturers and US cable operators announced the tru2way™ platform as a means to offer consumers easy access to high-definition service, video on demand (VOD) and two-way, interactive features.

“Industry consortiums supporting access through tru2way™ technology and devices like TriQuint’s new DOCSIS 3 IF SAW filter are making high speed, two-way television a reality, proof that growth in the digital TV market in China and around the world is continuing,” remarked Mr. Lin.

“TriQuint’s DOCSIS 3 IF SAW filter is a breakthrough product. This new device, together with our complete portfolio of RF power transistors, amplifiers, switches and filters for telecommunications, help us simplify connectivity for customers through an extensive, application-targeted product line. Those same techniques are now being used to design products for other applications which require wider bandwidths.”

TriQuint’s new IF SAW filter (p/n 856653) for DOCSIS 3.0 digital CATV systems is now sampling and shipping worldwide to major digital tuner and STB manufacturers. It is available in China through TriQuint offices in Shenzhen and Shanghai and throughout all of China by Avnet Asia Pacific.

For a detailed list of TriQuint RF products including gallium arsenide (GaAs) power amplifiers and transistors, LDMOS RF transistors, surface acoustic wave (SAW) and bulk acoustic wave (BAW) filters for wide-ranging telecommunications applications, visit http://www.triquint.com/china or www.triquint.com and register for new product details at www.triquint.com/china/rf or www.triquint.com/rf . To contact Avnet Asia Pacific, visit: http://www.avnet.com/home.

1. © October 2007 SeekingAlpha.com

2. DOCSIS and tru2way are trademarks of Cable Television Laboratories, Inc.

FORWARD LOOKING STATEMENTS
This TriQuint Semiconductor, Inc. (Nasdaq: TQNT) press release contains forward-looking statements made pursuant to the Safe Harbor provisions of the Private Securities Litigation Reform Act of 1995. Readers are cautioned that forward-looking statements involve risks and uncertainties. The cautionary statements made in this press release should be read as being applicable to all related statements wherever they appear. Statements containing such words as ‘leading’, ‘exceptional’, ‘high efficiency’, ‘adding value’, ‘leading supplier’, or similar terms are considered to contain uncertainty and are forward-looking statements. A number of factors affect TriQuint’s operating results and could cause its actual future results to differ materially from any results indicated in this press release or in any other forward-looking statements made by, or on behalf of, TriQuint including, but not limited to: those associated with the unpredictability and volatility of customer acceptance of and demand for our products and technologies, the ability of our production facilities and those of our vendors to meet demand, the ability of our production facilities and those of our vendors to produce products with yields sufficient to maintain profitability, as well as the other “Risk Factors” set forth in TriQuint’s most recent 10-Q report filed with the Securities and Exchange Commission. This and other reports can be found on the SEC web site, www.sec.gov. A reader of this release should understand that these and other risks could cause actual results to differ materially from expectations expressed / implied in forward-looking statements.

FACTS ABOUT TRIQUINT
Founded in 1985, we “Connect the Digital World to the Global Network”™ by supplying high-performance RF modules, components and foundry services to the world's leading communications companies. Specifically, TriQuint supplies products to four out of the top five cellular handset manufacturers, and is a leading gallium arsenide (GaAs) supplier to major defense and space contractors. TriQuint creates standard and custom products using advanced processes that include gallium arsenide, surface acoustic wave (SAW) and bulk acoustic wave (BAW) technologies to serve diverse markets including wireless handsets, base stations, broadband communications and military. TriQuint is also lead researcher in a 3-year DARPA program to develop advanced gallium nitride (GaN) amplifiers. TriQuint, as named by Strategy Analytics in August 2007, is the number-three worldwide leader in GaAs devices and the world’s largest commercial GaAs foundry. TriQuint has ISO9001 certified manufacturing facilities in Oregon, Texas, and Florida and a production plant in Costa Rica; design centers are located in North America and Germany. Visit TriQuint at www.triquint.com/rf to register for our newsletters.

Mr. Richard Lin
Director—Asia Sales
TriQuint Semiconductor, Inc.
Tel: +86-21-6886-3569
Mobile: +86-138-0199-7530
E-mail: rlin@tqs.com

Dr. Markus Behet
Networks Product Marketing Mgr.
TriQuint Semiconductor, Inc.
Tel: +49 8999626-2613
Mobile: +49 160-97260024
E-mail: mbehet@tqs.com

Media Contact:
Mr. Mark Andrews
Strategic MarComm Manager
TriQuint Semiconductor, Inc.
Tel: +1 (407) 884-3404
Mobile: +1 (407) 353-8727
E-mail: mandrews@tqs.com