Financial Releases
TriQuint Ramps New Filter Technology for 4G Mobile Hotspots and Smartphones
HILLSBORO, OREGON & ANAHEIM, CALIFORNIA (USA) – May 25, 2010 – TriQuint Semiconductor (NASDAQ: TQNT), a leading RF products manufacturer and foundry services provider, has released a family of new highly-selective WiFi / WiMAX RF bulk acoustic wave (BAW) 4G filters. TriQuint’s BAW filters enable mobile devices to act as portable WLAN (WiFi) hotspots, and simultaneously connect directly to 4G WiMAX networks for broadband access up to 10 times faster than conventional 3G systems.
TriQuint’s innovative new filters give WLAN handsets, laptops and similar products fully-mobile, high-speed WiMAX access. Individuals can use 4G WiMAX to more quickly download movies, stream video or connect with interactive gaming. Wireless system operators including Sprint Clearwire offer 4G WiMAX devices and service across more than 20 markets in the US; there are over 550 WiMAX service areas worldwide.
Mobile devices with TriQuint BAW filter technology like the Sierra Wireless AirCard® W801 Mobile Hotspot (available from Sprint as the Overdrive™ 3G/4G mobile hotspot) can provide WLAN access for up to 5 connected devices. Through the AirCard W801, users may also directly access 4G WiMAX networks with their WiFi-enabled smartphone or laptop.
“The Sierra Wireless AirCard W801 Mobile Hotspot combines WiFi and WiMAX into a single device to allow users to connect multiple WiFi-equipped devices – such as phones, laptops, or ebook readers – to the internet over 4G broadband connections. Since WiMAX and WiFi are adjacent in the RF spectrum, TriQuint’s highly-selective filters reduce interference and let mobile devices that use both frequencies, like the AirCard W801 mobile hotspot, deliver dependable service,” said Evan Jones, Vice President of Engineering for Sierra Wireless.
Remarking on the critical role played by filtering in the emerging 4G WiMAX market, TriQuint Vice President Brian Balut said that without highly-selective BAW devices a “personal hot spot” would interfere with itself, severing wireless connections or otherwise rendering them unusable.
“TriQuint has developed a wide range of WiMAX and WiFi products for laptops and hand-held mobile devices that simplify RF connectivity,” Mr. Balut said. “Our latest products leverage TriQuint’s long-standing filter expertise and BAW innovations by shielding one frequency band from another, making them both fully accessible. Having this flexibility helps end users upload and download very large files very quickly. The flexibility to access WiMAX networks with an existing 3G smartphone or WiFi laptop gives consumers 4G access while extending the lifetime of their existing mobile device—it’s transformational technology,” he added.
Personal hotspots such as those enabled by TriQuint BAW technology are expected by market analysts to create a new segment in the 3G/4G mobile broadband sector. Market watchers including Strategy Analytics have indicated that hotspot products should see increasing consumer demand.
“The devices that opened this branch of the mobile hotspot market were 3G; 4G devices were more recently introduced, so this market is beginning to evolve,” remarked Chris Taylor, director, Strategy Analytics RF & Wireless Components. “Bringing 4G connections to existing 3G devices, and having the ability to access 4G by new generations of wireless and RF-enabled laptops could create an opportunity for rapid expansion; this expansion will help satisfy the growing consumer demand for faster wireless mobile broadband access.”
WiMAX markets today include 52 areas in the US and Canada; there are 568 worldwide. WiMAX service areas are increasing quickly according to the WiMAX Forum®, an international trade group. This is especially true in areas where quality 3G service is absent, or service quality is declining because networks are not keeping pace with subscriber growth. By offering service up to 10 times faster than 3G, 4G WiMAX service growth will accelerate, predicts the Forum.
Technical Details
TriQuint’s filter technology leadership is based on more than two decades of surface acoustic wave (SAW), temperature compensated (TC) SAW and bulk acoustic wave (BAW) innovation. SAW devices offer market-tested reliability for mobile and base station applications through 1.5 GHz. TriQuint integrated and discrete SAW devices have excelled in multiple mobile communications and broadband data markets based on their ability to offer cost-sensitive filter solutions while reducing insertion loss (greater filter efficiency) and providing the bandwidth and steepness (the ability to affect a precise signal area) that RF designers require.
TriQuint BAW filters are designed for high performance at frequencies greater than 1.5 GHz. BAW technology is particularly adept at solving complex filter challenges such as enabling adjacent bands in the RF spectrum to function at the same time without interference. BAW’s ability to provide steep rolloff enables one filter to reject near-in interference while maintaining excellent, low loss performance.
New high frequency WiMAX/WiFi filters from TriQuint are featured in bills of materials by today’s major WiMAX chipset reference designers including Sequans, Beceem and GCT. The filters exhibit extremely steep roll-off between passbands and rejection bands, which is the key performance factor for enabling devices that must simultaneously use WiFi and WiMAX signals.
|
885007 |
2.4 GHz ISM/WiFi passband filter with low loss and extreme steepness. The rejection band starts at the lower edge of the worldwide WiMAX/LTE band: 2496 MHz. |
|
885008 |
2.4 GHz ISM/WiFi ‘notch’ filter that rejects the WiFi band while maintaining low loss across the entire 2.496-2.69 GHz worldwide WiMAX/LTE band. |
|
885010 |
2.4 GHz ISM/WiFi/BT ‘notch’ filter that rejects the entire WiFi/BT band from 2.4 to 2.483 GHz, while passing the bands above and below this notch. This includes the WCS/WiBRO band (2.305-2.36 GHz) as well as the worldwide WiMAX/LTE band (2.496-2.69 GHz). |
TriQuint’s new filters, amplifiers and integrated products for simplified RF connectivity including devices based on BAW, SAW, GaN and GaAs technology will be on display at the IEEE IMS MTT-S Symposium and Exhibition in Anaheim, CA, (May 25-27), Booth 1724.
For more information about TriQuint’s new WiMAX / WLAN filter solutions and other mobile device products, contact TriQuint Product Marketing or visit us on the web at: www.triquint.com. For information about future product releases and to subscribe to our newsletter, visit www.triquint.com/rf.
Forward-Looking Statements:
This TriQuint Semiconductor, Inc. (NASDAQ: TQNT) press release contains forward-looking statements made pursuant to the Safe Harbor provisions of the Private Securities Litigation Reform Act of 1995. Readers are cautioned that forward-looking statements involve risks and uncertainties. The cautionary statements made in this press release should be read as being applicable to all related statements wherever they appear. Statements containing such words as ‘leading’, ‘exceptional’, ‘high efficiency’, ‘key role’, ‘leading supplier’, or similar terms are considered to contain uncertainty and are forward-looking statements. A number of factors affect TriQuint’s operating results and could cause its actual future results to differ materially from any results indicated in this press release or in any other forward-looking statements made by, or on behalf of, TriQuint including, but not limited to: those associated with the unpredictability and volatility of customer acceptance of and demand for our products and technologies, the ability of our production facilities and those of our vendors to meet demand, the ability of our production facilities and those of our vendors to produce products with yields sufficient to maintain profitability, as well as the other “Risk Factors” set forth in TriQuint’s most recent 10-Q report filed with the Securities and Exchange Commission. This and other reports can be found on the SEC web site, www.sec.gov. A reader of this release should understand that these and other risks could cause actual results to differ materially from expectations expressed / implied in forward-looking statements.
Facts About TriQuint
TriQuint Semiconductor (NASDAQ: TQNT) celebrates its 25th anniversary in 2010 as a leading global provider of innovative RF solutions and foundry services for the world’s leading communications, defense and aerospace companies. People and organizations around the world need real-time, all-the-time connections; TriQuint products help reduce the cost and increase the performance of connected mobile devices and the networks that deliver critical voice, data and video communications. With the industry’s broadest technology portfolio, recognized R&D leadership, and expertise in high-volume manufacturing, TriQuint creates standard and custom products using gallium arsenide (GaAs), gallium nitride (GaN), surface acoustic wave (SAW) and bulk acoustic wave (BAW) technologies. The company has ISO9001-certified manufacturing facilities in the U.S., production in Costa Rica, and design centers in North America and Germany. For more information, visit www.triquint.com.
TriQuint: Connecting the Digital World to the Global Network®
|
TriQuint Product Marketing: Joshua Raha |
TriQuint Media Contact: Mark Andrews |