Financial Releases
RFMD(R) Unveils First 1.2 GHz Power Doubler Amplifier Supporting New DOCSIS 3.1 Cable Specification
RFMD's new Gallium Nitride- (GaN-) based RFCM3316 allows cable operators and MSOs to easily upgrade existing CATV infrastructure to meet the power amplifier requirements of the new DOCSIS 3.1 standard, increasing effective downstream data rates from 160 Megabits per second (Mb/s) to 10 Gigabits per second (Gbit/s), and upstream data rates from 120 Mb/s to 1 Gbit/s when compared to DOCSIS 3.0. Due to the high output and gain benefits derived from RFMD's GaN-based RFCM3316, cable operators can upgrade their existing equipment within current locations, saving on both installation time and cost.
"Our new power doubler amplifier solution underscores RFMD's product leadership by creating an easy upgrade to the DOCSIS 3.1 standard for CATV operators and MSOs, extending the life of existing networks," said
The RFCM3316 operates from 40MHz to 1200MHz and provides an extremely high output level of 60dBmV under a 1.2GHz channel loading with < 10-10 BER and 42dB MER and -80dB CTB and -80dB CSO. This modular, surface mount device saves about 50 percent in board space compared to traditional SOT115J packages, while maintaining excellent linearity and ruggedness. Due to the efficient nature of the GaN process, the product can also operate at 20% less current than Gallium Arsenide-based products at a comparable distortion level.
The RFCM3316 is now sampling with key customers, and volume production is expected to begin in the first quarter of 2014. RFCM3316 is the newest addition to RFMD's differential amplifier family developed for CATV transmission that includes power doublers and push-pull amplifiers delivering unmatched performance in terms of output power, bandwidth, linearity, current consumption and reliability. RFMD will showcase its portfolio of industry-leading CATV components at its booth (#1362) at the SCTE Cable-Tec Expo to be held in
About RFMD
This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these
forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws.
CONTACT: At RFMD(R)
Doug DeLieto
VP, Investor Relations
336-678-5322
Media Contact
Brent Dietz
Director of Corporate Communications
336-678-7935
brent.dietz@rfmd.com
Source: News Provided by Acquire Media