LAS VEGAS, Jan. 8, 2013 (GLOBE NEWSWIRE) -- RF Micro Devices, Inc. (Nasdaq:RFMD), a global leader in the design and manufacture of high-performance radio frequency components, announced today it will unveil a highly-integrated front end module (FEM) for Smart Energy/Advanced Metering Infrastructure (AMI) applications at the 2013 Consumer Electronics Show (CES) in Las Vegas. RFMD's single-chip RFFM6403 FEM delivers industry-leading performance, reduces customer design time and speeds customer time-to-market in Smart Energy/AMI applications operating in the 405MHz—475MHz frequency range, as well as for portable battery powered equipment and general 433/470MHz ISM band systems.
The feature-rich RFFM6403 integrates a transmit high power path with a +30.5dBm PA and Tx harmonic output filtering, a transmit bypass thru path with Tx harmonic output filtering, and a receive path with a low noise amplifier (LNA) with bypass mode. The FEM also features a low insertion loss/high isolation SP3T switch and separate Rx/Tx 50 ohm ports, simplifying matching and providing input and output signals for both the Tx and Rx paths.
The RFFM6403 is designed for AMI systems operating with high efficiency requirements and a minimum output power of 30 dBm. In the receive path, the Rx chain provides 16 dB of typical gain with only 5 mA of current and an excellent noise figure of 1.7 dB. The high level of integration and industry-leading form factor (6mm x 6mm x 1mm) minimize product footprint at the customer device while reducing external component count and associated assembly costs.
RFMD will showcase its broad portfolio of Smart Energy/AMI, ZigBee, and ISM band solutions from January 8 to January 11, at the 2013 Consumer Electronics Show in the ZigBee Alliance Pavilion, in South Hall 1, booth 20612, at the Las Vegas Convention Center.
About RFMD
RF Micro Devices, Inc. (Nasdaq:RFMD) is a global leader in the design and manufacture of high-performance radio frequency components. RFMD's products enable worldwide mobility, provide enhanced connectivity and support advanced functionality in the mobile device, wireless infrastructure, wireless local area network (WLAN or WiFi), cable television (CATV)/broadband, Smart Energy/advanced metering infrastructure (AMI), and aerospace and defense markets. RFMD is recognized for its diverse portfolio of semiconductor technologies and RF systems expertise and is a preferred supplier to the world's leading mobile device, customer premises and communications equipment providers.
Headquartered in Greensboro, N.C., RFMD is an ISO 9001-, ISO 14001-, and ISO/TS 16949-certified manufacturer with worldwide engineering, design, sales and service facilities. RFMD is traded on the NASDAQ Global Select Market under the symbol RFMD. For more information, please visit RFMD's web site at www.rfmd.com.
The RF Micro Devices, Inc. logo is available at http://www.globenewswire.com/newsroom/prs/?pkgid=6436
This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these
forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. RF Micro Devices' business is subject to numerous risks and uncertainties, including risks associated with the impact of global macroeconomic and credit conditions on our business and the business of our suppliers and customers, variability in operating results, the rate of growth and development of wireless markets, our reliance on inclusion in third party reference designs for a portion of our revenue, our ability to manage channel partner and customer relationships, risks associated with the operation of our wafer fabrication, molecular beam epitaxy, assembly and test and tape and reel facilities, our ability to complete acquisitions and integrate acquired
companies, including the risk that we may not realize expected synergies from our business combinations, our ability to attract and retain skilled personnel and develop leaders, variability in production yields, raw material costs and availability, our ability to reduce costs and improve margins in response to declining average selling prices, our ability to bring new products to market, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, dependence on a limited number of customers, dependence on gallium arsenide (GaAs) for the majority of our products, and dependence on third parties. These and other risks and uncertainties, which are described in more detail in RF Micro Devices' most recent Annual Report on Form 10-K and other reports and statements filed with the
Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.
RF MICRO DEVICES® and RFMD® are trademarks of RFMD, LLC. All other trade names, trademarks and
registered trademarks are the property of their respective owners.
CONTACT: At RFMD
Doug DeLieto
VP, Investor Relations
336-678-7088
Source:
RF Micro Devices
News Provided by Acquire Media