Financial Releases
RFMD Introduces RF5365 WiFi Front End Module
GREENSBORO, N.C., Jul 13, 2010 (GlobeNewswire via COMTEX News Network) -- RF Micro Devices, Inc. (Nasdaq:RFMD), a global leader in the design and manufacture of high-performance radio frequency components and compound semiconductor technologies, today announced availability of the RF5365 WiFi front end module (FEM). The highly integrated RF5365 FEM satisfies the need for aggressive size reductions for typical 802.11b/g front-end designs and greatly reduces the number of components outside the core chipset.
RFMD's RF5365 FEM integrates a 802.11b/g power amplifier with a single pole three throw (SP3T) switch for 2.4 GHz to 2.5 Ghz ISM band applications. By integrating SP3T switch functionality, the RF5365 is able to route WLAN and Bluetooth(R) receive/transmit signals to two system-on-chip (SOC) transceivers, accommodating a common implementation in high-performance consumer electronics and handset/handheld WiFi applications. The SP3T switch can also act as a splitter to transmit or receive Bluetooth(R) and WLAN signals simultaneously.
The RF5365's 802.11 b/g power amplifier delivers 18dBm of linear output power for higher efficiency and lower EVM for 11n applications. Additionally, integrated 2170MHz filtering and harmonic attenuation reduce the need for a high loss/attenuation filter at the FEM output, increasing output power at the antenna.
An integrated Rx balun eliminates requirements for tuning components between the FEM and the SoC, and a direct-to-battery connection eliminates the need for additional DC circuitry. Finally, an integrated power detector increases immunity to power supply, temperature and VSWR fluctuations and improves the accuracy of the part's closed loop power control. The RF5365 is fully tested and packaged in a small 2.5 mm x 2.5 mm QFN package.
About RFMD
RF Micro Devices, Inc. (Nasdaq:RFMD) is a global leader in the design and manufacture of high-performance radio frequency components and compound semiconductor technologies. RFMD's products enable worldwide mobility, provide enhanced connectivity and support advanced functionality in the cellular handset, wireless infrastructure, wireless local area network (WLAN), CATV/broadband and aerospace and defense markets. RFMD is recognized for its diverse portfolio of semiconductor technologies and RF systems expertise and is a preferred supplier to the world's leading mobile device, customer premises and communications equipment providers.
Headquartered in Greensboro, N.C., RFMD is an ISO 9001- and ISO 14001-certified manufacturer with worldwide engineering, design, sales and service facilities. RFMD is traded on the NASDAQ Global Select Market under the symbol RFMD. For more information, please visit RFMD's web site at www.rfmd.com.
The RF Micro Devices, Inc. logo is available at http://www.globenewswire.com/newsroom/prs/?pkgid=6436
This press release includes "forward-looking statements" within the meaning of the safe harbor provisions of the Private Securities Litigation Reform Act of 1995. These forward-looking statements include, but are not limited to, statements about our plans, objectives, representations and contentions and are not historical facts and typically are identified by use of terms such as "may," "will," "should," "could," "expect," "plan," "anticipate," "believe," "estimate," "predict," "potential," "continue" and similar words, although some forward-looking statements are expressed differently. You should be aware that the forward-looking statements included herein represent management's current judgment and expectations, but our actual results, events and performance could differ materially from those expressed or implied by forward-looking statements. We do not intend to update any of these forward-looking statements or publicly announce the results of any revisions to these forward-looking statements, other than as is required under the federal securities laws. RF Micro Devices' business is subject to numerous risks and uncertainties, including risks associated with the impact of global macroeconomic and credit conditions on our business and the business of our suppliers and customers, variability in operating results, the rate of growth and development of wireless markets, our reliance on inclusion in third party reference designs for a portion of our revenue, our ability to manage channel partner and customer relationships, risks associated with the operation of our wafer fabrication, molecular beam epitaxy, assembly and test and tape and reel facilities, our ability to complete acquisitions and integrate acquired companies, including the risk that we may not realize expected synergies from our business combinations, our ability to attract and retain skilled personnel and develop leaders, variability in production yields, raw material costs and availability, our ability to reduce costs and improve margins in response to declining average selling prices, our ability to bring new products to market, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, dependence on a limited number of customers, dependence on gallium arsenide (GaAs) for the majority of our products, and dependence on third parties. These and other risks and uncertainties, which are described in more detail in RF Micro Devices' most recent Annual Report on Form 10-K and other reports and statements filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.
RF MICRO DEVICES(R) and RFMD(R) are trademarks of RFMD, LLC. All other
trade names, trademarks and registered trademarks are the property of
their respective owners.
This news release was distributed by GlobeNewswire, www.globenewswire.com
SOURCE: RF Micro Devices
CONTACT: RF Micro Devices Douglas DeLieto, VP of Investor Relations 336-678-7088
(C) Copyright 2010 GlobeNewswire, Inc. All rights reserved.
News Provided by COMTEX