Financial Releases

RF Micro Devices(R) and Nujira Partner to Create the World's Most Efficient Broadband Power Amplifier

CAMBRIDGE, U.K., and GREENSBORO, N.C., Feb 3, 2010 (GlobeNewswire via COMTEX News Network) -- Nujira and RF Micro Devices, Inc. (Nasdaq:RFMD), a global leader in the design and manufacture of high-performance radio frequency components and compound semiconductor technologies, today announced that they will be demonstrating the world's most efficient broadband power amplifier (PA) design for 4G base stations at Mobile World Congress, Barcelona, February 2010. The design integrates the new RFMD RFG1M family of high performance gallium nitride (GaN) amplifiers with Nujira's Coolteq.h envelope tracking power modulators.

Using just one RFG1M device with a Coolteq.h module, the RFMD Nujira RF front end transmits over a 728 -- 960 MHz band with over 50% efficiency, covering seven of the frequency bands defined for LTE by 3GPP. The results of this broadband GaN-based PA platform surpass competitive wideband Doherty LDMOS solutions. Furthermore, using future GaN devices currently in development at RFMD, the two companies expect to cover the full range of the cellular frequency band from 700 MHz -- 2,600 MHz with just three broadband PAs, allowing wireless infrastructure vendors to develop a single, highly-efficient multimode, broadband RF front end that can be deployed to meet various transmission standards anywhere in the world.

Lance Wilson, Research Director, RF Components & Systems, ABI Research, said, "Expect to see GaN, coupled with envelope tracking, in many new RRH designs. With a GaN/envelope tracking amplifier promising such high-efficiency operation, the Doherty circuit configuration can be disposed of and bandwidth will increase incrementally." (ABI Research, Remote Radio Heads, Q4 2009)

Commenting, Tim Haynes, CEO, Nujira said, "In partnership with RFMD, we have created a PA which covers the entire 700 MHz -- 1000 MHz band without compromising on efficiency. Nujira's Coolteq modulators feature the only technology that can deliver this level of efficiency across such a broad bandwidth, extending the Software Defined Radio approach to the high-value power amplifier."

Bob Van Buskirk, president of RFMD's Multi-Market Products Group (MPG), said, "We're delighted to be collaborating with Nujira in setting new standards for energy efficient transmission performance based on our new RFG1M products and on our state-of-the-art GaN process. We see the combination of Envelope Tracking and RFMD's superior GaN devices and technology as a disruptive combination that changes the way base stations are designed."

According to Haynes, the joint design addresses a major issue in the 4G cellular base station market. "Infrastructure vendors are facing a portfolio management crisis, with more than 60 product variants needed to cover all worldwide frequency bands, cellular standards, and power levels," he said. "Even if they had the specialist engineering resources available to develop each product, the development costs and timescales would be prohibitive, with each and every variant costing hundreds of thousands of dollars to design, test, type approve, and qualify for production. We have delivered a high efficiency, broadband PA platform which can be deployed across multiple product variants, reducing time-to-market, development costs, and the cost of ownership associated with inventory management."

The design is based on RFMD's RFG1M09180 180W GaN broadband power transistor. RFMD's GaN devices can provide high efficiency across a broad RF bandwidth, enabling the entire cellular spectrum (from 700 MHz to 2700 MHz) to be covered with a reduced number of PA platforms.

About RFMD

RF Micro Devices, Inc. (Nasdaq:RFMD) is a global leader in the design and manufacture of high-performance radio frequency components and compound semiconductor technologies. RFMD's products enable worldwide mobility, provide enhanced connectivity and support advanced functionality in the cellular handset, wireless infrastructure, wireless local area network (WLAN), CATV/broadband and aerospace and defense markets. RFMD is recognized for its diverse portfolio of semiconductor technologies and RF systems expertise and is a preferred supplier to the world's leading mobile device, customer premises and communications equipment providers.

Headquartered in Greensboro, N.C., RFMD is an ISO 9001- and ISO 14001-certified manufacturer with worldwide engineering, design, sales and service facilities. RFMD is traded on the NASDAQ Global Select Market under the symbol RFMD. For more information, please visit RFMD's web site at www.rfmd.com.

The RF Micro Devices, Inc. logo is available at http://www.globenewswire.com/newsroom/prs/?pkgid=6436

About Nujira

Nujira's mission is to dramatically improve the energy efficiency of transmitters for digital cellular and broadcast transmitters by reducing the amount of waste energy dissipated as heat in the RF Power Amplifier circuit. Nujira High Accuracy Tracking (HAT(TM)) Modulator technology dynamically controls the power supply to the circuit in line with the transmission performance required, enabling the creation of highly efficient RF Power Amplifiers for 3G and 4G cellular base stations, handsets and TV broadcast transmitters.

For further details see www.nujira.com.

Nujira Limited, Building 1010, Cambourne Business Park, Cambourne, Cambridge, United Kingdom, CB23 6DP, Telephone: +44 1223 597900, Fax: +44 1223 597972

This news release was distributed by GlobeNewswire, www.globenewswire.com

SOURCE: RF Micro Devices; Nujira Limited

CONTACT:  Neesham PR
For Nujira:
Peter van der Sluijs
+44 1296 628180
peterv@neesham.co.uk
RF Micro Devices
Douglas DeLieto, Vice President, Investor Relations
(336) 678-7088

(C) Copyright 2010 GlobeNewswire, Inc. All rights reserved.

News Provided by COMTEX