Financial Releases

RF Micro Devices Extends Traction in Cellular Handset Market with Optimized Bluetooth Hardware and Advanced Software Solutions

RF Micro Devices Extends Traction in Cellular Handset Market with Optimized Bluetooth Hardware and Advanced Software Solutions

RFMD's UltimateBlue™ Portfolio Enables New Class of Bluetooth Applications For Next-Generation Cellular Handsets

LONDON--(BUSINESS WIRE)--May 24, 2005--RF Micro Devices®, Inc. (NASDAQ: RFMD)®, a leading provider of proprietary radio frequency integrated circuits (RFICs) for wireless communications applications, today announced that it has extended its traction in the cellular handset market with its complete line of system-on-chip (SoC) Bluetooth® products, transceivers and protocol stack software, enabling handset manufacturers to more easily integrate Bluetooth wireless technology into current- and next-generation cellular handsets. RFMD's UltimateBlue™ solutions are optimized to deliver advanced capabilities, such as Enhanced Data Rate (EDR) and streaming music that leading cellular service providers are requiring in their feature-rich handsets.

Frank Morese, vice president, Wireless Connectivity Business Unit, RFMD, said, "RFMD's Bluetooth solutions continue to gain traction in the high-volume market for cellular handsets. Our Bluetooth solutions have been qualified for numerous phone designs, and we expect multiple new handsets will incorporate our Bluetooth solutions this year. This summer, we anticipate that shipments will commence to major handset manufacturers."

David Favreau, general manager, Wireless Personal Networking (WPAN) product line at RFMD, said, "The advent of mobile phones with MP3 playback and storage capabilities is driving increased demand for Bluetooth technology. Through the advanced audio/video capabilities of our Bluetooth solutions, RFMD is giving consumers the freedom to experience CD-quality audio via wireless headset connections to their mobile phones. RFMD will continue to meet the growing demand for Bluetooth technology in cell phones through the reduced system cost of our on-board solutions and the migration to EDR capabilities."

RFMD offers a complete line of high-performance, low-power Bluetooth SoC solutions for mobile phones. The Company also offers feature-rich HCI software, upper layer protocol stack software, all major profiles and development tools that enable customers to speed their products to market.

RFMD's UltimateBlue Bluetooth portfolio is comprised of the following solutions:

    --  The SiW4000 SoC Bluetooth solution with EDR is the world's
        smallest Bluetooth EDR solution in 0.13 micron with
        best-in-class current consumption. With its easy-to-use 4.5mm
        x 4.5mm BGA package, low power consumption and low bill of
        materials (BOM) cost, the SiW4000 is ideally suited for
        high-volume mobile phone production. The SiW4000 is being
        featured at Wireless Connectivity World 2005.

    --  The SiW3500 SoC Bluetooth solution is Bluetooth V2.0 qualified
        for improved interoperability with existing Bluetooth
        products. The on-chip RF matching circuit facilitates direct
        on-board design, accelerating time to market while lowering
        the cost of implementation. The SiW3500 is currently shipping
        in volume to handset original equipment manufacturers (OEMs).

    --  The SiW1722 transceiver is specifically designed and
        OEM-qualified for Bluetooth-enabled CDMA mobile phone ASICs.
        Leveraging the Bluetooth baseband function integrated into the
        mobile phone ASIC, this solution provides the lowest total
        cost to add Bluetooth technology into a mobile phone design.
        The SiW1722 is Bluetooth V2.0 qualified and is in production
        now.

    --  RFMD's embedded protocol stack and profile software delivers a
        flexible solution that is easily ported to mobile phone
        platforms. More than 20 individual profiles are available,
        such as stereo audio profile (A2DP) and remote control profile
        (AVRCP), which are being requested by an increasing number of
        carriers. With its well-defined programming interface, porting
        to the mobile phone platform can be accomplished with
        confidence. RFMD offers a turnkey mobile phone solution via
        the Embedded Host Software Development Kit (SDK).

Please visit RFMD at Wireless Connectivity World 2005 in London, May 24-25, 2005, booth #220 to view its Bluetooth portfolio and other wireless connectivity solutions for WLAN and GPS.

RF Micro Devices, Inc., an ISO 9001- and ISO 14001-certified manufacturer, designs, develops, manufactures and markets proprietary radio frequency integrated circuits (RFICs) for wireless communications products and applications. The Company is a leading supplier of power amplifiers, one of the most critical radio frequency (RF) components in cellular phones. The Company is also the leading manufacturer of GaAs HBT, which offers distinct advantages over other technologies for the manufacture of current- and next-generation power amplifiers. The Company's products are included primarily in cellular phones, base stations, wireless local area networks (WLANs), cable television modems and global positioning systems (GPS). The Company derives revenue from the sale of standard and custom-designed products. The Company offers a broad array of products including amplifiers, mixers, modulators/demodulators and single-chip transmitters, Bluetooth® products and receivers and transceivers that represent a substantial majority of the RFICs required in wireless subscriber equipment. The Company's goal is to be the premier supplier of low-cost, high-performance integrated circuits and solutions for applications that enable wireless connectivity. RF Micro Devices, Inc., is traded on the Nasdaq National Market under the symbol RFMD. For more information about RFMD, please visit www.rfmd.com.

This press release contains forward-looking statements that relate to RF Micro Devices' plans, objectives, estimates and goals. Words such as "expects," "anticipates," "intends," "plans," "projects," "believes" and "estimates," and variations of these words and similar expressions, identify these forward-looking statements. RF Micro Devices' business is subject to numerous risks and uncertainties, including variability in quarterly operating results, the rate of growth and development of wireless markets, risks associated with the operation of wafer fabrication, molecular beam epitaxy and other foreign and domestic manufacturing facilities, our ability to attract and retain skilled personnel and develop leaders, variability in production yields, our ability to reduce costs and improve gross margins by implementing innovative technologies, our ability to bring new products to market, our ability to adjust production capacity in a timely fashion in response to changes in demand for our products, dependence on a limited number of customers and dependence on third parties. These and other risks and uncertainties, which are described in more detail in RF Micro Devices' most recent Annual Report on Form 10-K filed with the Securities and Exchange Commission, could cause actual results and developments to be materially different from those expressed or implied by any of these forward-looking statements.

RF MICRO DEVICES®, RFMD® and UltimateBlue™ are trademarks of RFMD, LLC.

BLUETOOTH is a trademark owned by Bluetooth SIG, Inc., U.S.A. and licensed for use by RF Micro Devices, Inc.

CONTACT: RF Micro Devices
Jerry Neal, 336-664-1233

SOURCE: RF Micro Devices