Meet TriQuint's Experts at IMS 2011 and Discover New Ways to Lower Power
Consumption and Prevent Network System ESD, RF Over-Drive & DC
Over-Voltage Failures
BALTIMORE & HILLSBORO, Ore.--(BUSINESS WIRE)--
TriQuint Semiconductor (NASDAQ:TQNT), a leading RF solutions supplier
and technology innovator, has released the first members in a new family
of integrated RF products that lower power consumption while protecting
mobile networks from disruption and service failures. TriQuint's newest
base transceiver station (BTS) network devices join 12 other new power
and filter infrastructure solutions introduced in the first half of 2011.
"We listened to our customers in developing these products," said Vice
President Brian P. Balut. "Consumer demand for smartphones and tablets
means more bandwidth through the network. That leads to the requirement
for greater linearity in the RF chain. At the same time, our customers
want to minimize power consumption, and they want devices that withstand
spikes and other stresses that may occur in the field. These two new
products uniquely address all these needs."
TriQuint is focused on bringing performance innovation to essential
building blocks in the global network. This network is fraught with
demand, and it's not going to let up; by 2015, the amount of mobile data
traffic contributed by tablets alone is expected to equal that of mobile
data traffic from all devices combined in 2010.*
TriQuint's new base station devices, starting with the 0.25 Watt
TQP7M9101, provides high gain and linearity with very low current
consumption—just 88 mA (milliamps) in a typical 5 Volt design. The 0.5
Watt TQP7M9102 is also now available; it provides highly-linear
performance, low current consumption and greater gain.
Setting these amplifiers apart from others now available is TriQuint's
patent-pending integrated protection features that include means to
guard against ESD and DC over-voltage electrical spikes. TriQuint also
integrates RF over-drive protection that reduces the chance of damage
from high signal levels often seen in systems employing digital
pre-distortion linearization techniques commonly utilized to meet 3G/4G
BTS system requirements. Unlike other linear driver amplifiers available
today, TriQuint's TQP7M9101 also integrates matching circuits that
eliminate the need externally. These integration benefits reduce the
overall BOM and provide easier-to-use solutions that are especially
important when fast time-to-market is a key manufacturer strategy.
"TriQuint regularly releases new amplifier and linear gain blocks that
offer useful improvements. They appreciate that design requirements
change all the time," said Alexander Kopp, RF designer, Andrew Wireless
Systems / CommScope, Buchdorf, Germany. "A more linear RF signal is very
important, and with very low current drain, we can reduce a system's
thermal dissipation. The TriQuint team has offered us great support."
TriQuint's two new amplifiers are ideal for 3G/4G wireless
infrastructure applications including base transceiver stations,
repeaters, boosters, tower-mounted amplifiers (TMAs), remote radio
heads, defense/aerospace and other wireless systems requiring high
linearity and gain with low power consumption.
TriQuint's base station, microwave and defense/aerospace innovations
will be displayed at the IEEE IMS / MTT-S Conference and Exhibition
(June 5-10, Baltimore, Maryland.) Visit TriQuint at Booth #2218, or
request a meeting with our experts at: info-networks@tqs.com.
For information about future product releases and to subscribe to our
newsletter, visit www.triquint.com/rf.
*Source: 2011 Cisco Visual Networking Index
Technical Details
|
TQP7M9101
|
|
0.25W high-linearity amplifier. Performance at 2.1 GHz: 17.5 dB
gain, 40 dBm OIP3 & 24.8 dBm P1dB while consuming only 88 mA current
from a 5V supply. Integrated RF over-drive, DC over-voltage and
Class 2 (2000V) HBM ESD protection.
|
|
TQP7M9102
|
|
0.5W high-linearity amplifier. Performance at 2.1 GHz: 17.8 dB gain,
43.5 dBm OIP3 & 27.5 dBm P1dB while consuming only 137 mA current
from a 5V supply. Integrated RF over-drive, DC over-voltage and
Class 2 (2000V) HBM ESD protection.
|
FORWARD LOOKING STATEMENTS
This TriQuint Semiconductor, Inc. (NASDAQ:TQNT) press release
contains forward-looking statements made pursuant to the Safe Harbor
provisions of the Private Securities Litigation Reform Act of 1995.
Readers are cautioned that forward-looking statements involve risks and
uncertainties. The cautionary statements made in this press release
should be read as being applicable to all related statements wherever
they appear. Statements containing such words as ‘leading',
‘exceptional', ‘high efficiency', ‘key role', ‘leading supplier', or
similar terms are considered to contain uncertainty and are
forward-looking statements. A number of factors affect TriQuint's
operating results and could cause its actual future results to differ
materially from any results indicated in this press release or in any
other forward-looking statements made by, or on behalf of, TriQuint
including, but not limited to: those associated with the
unpredictability and volatility of customer acceptance of and demand for
our products and technologies, the ability of our production facilities
and those of our vendors to meet demand, the ability of our production
facilities and those of our vendors to produce products with yields
sufficient to maintain profitability, as well as the other "Risk
Factors" set forth in TriQuint's most recent 10-Q report filed with the
Securities and Exchange Commission. This and other reports can be found
on the SEC web site, www.sec.gov.
A reader of this release should understand that these and other risks
could cause actual results to differ materially from expectations
expressed / implied in forward-looking statements.
FACTS ABOUT TRIQUINT
Founded in 1985, TriQuint Semiconductor (NASDAQ:TQNT) is a leading
global provider of innovative RF solutions and foundry services for the
world's top communications, defense and aerospace companies. People and
organizations around the world need real-time, all-the-time connections;
TriQuint products help reduce the cost and increase the performance of
connected mobile devices and the networks that deliver critical voice,
data and video communications. With the industry's broadest technology
portfolio, recognized R&D leadership, and expertise in high-volume
manufacturing, TriQuint creates standard and custom products using
gallium arsenide (GaAs), gallium nitride (GaN), surface acoustic wave
(SAW) and bulk acoustic wave (BAW) technologies. The company has
ISO9001-certified manufacturing facilities in the U.S., production in
Costa Rica, and design centers in North America and Germany. For more
information, visit www.triquint.com.
TriQuint: Connecting the Digital World to the Global Network®
Photos/Multimedia Gallery Available: http://www.businesswire.com/cgi-bin/mmg.cgi?eid=6749044&lang=en

TriQuint Semiconductor, Inc.
TriQuint Product Marketing:
Doug
Slansky, +1-972-994-8285
Product Marketing Director
dslansky@tqs.com
or
TriQuint
Media Contact:
Mark Andrews, +1-407-884-3404
Strategic
Marketing Communications Mgr.
Mobile : +1-407-353-8727
mandrews@tqs.com
Source: TriQuint Semiconductor
News Provided by Acquire Media